Camozzi news

 
 
 
Menu

 

Camozzi news

MECSPE 2022: Camozzi Group and the Italian Institute of Technology have won the "Solution Award"

10.06.22
Projects
di lettura

The robotic system for the monitoring and maintenance of the San Giorgio Bridge, designed by the Camozzi Group and the Italian Institute of Technology, has won the "๐‘ฐ๐’๐’๐’๐’—๐’‚๐’•๐’Š๐’๐’ ๐’‚๐’๐’… ๐‘น๐’๐’ƒ๐’๐’•๐’Š๐’„๐’”" award in the category of "๐’ƒ๐’†๐’”๐’• ๐’Š๐’๐’…๐’–๐’”๐’•๐’“๐’Š๐’‚๐’ ๐’๐’“ ๐’”๐’†๐’“๐’—๐’Š๐’„๐’† ๐’“๐’๐’ƒ๐’๐’•๐’Š๐’„๐’” ๐’‚๐’‘๐’‘๐’๐’Š๐’„๐’‚๐’•๐’Š๐’๐’"

The awards event for the winners of the "Solution Award" was held on Friday, June 10th, 2022, during the MECSPE exhibition, at the Bologna Fiere Service Center.

The Robotic System for the Monitoring and Maintenance of the San Giorgio Bridge in Genoa has won the "๐‘ฐ๐’๐’๐’๐’—๐’‚๐’•๐’Š๐’๐’ ๐’‚๐’๐’… ๐‘น๐’๐’ƒ๐’๐’•๐’Š๐’„๐’”" award in the category of "๐’ƒ๐’†๐’”๐’• ๐’Š๐’๐’…๐’–๐’”๐’•๐’“๐’Š๐’‚๐’ ๐’๐’“ ๐’”๐’†๐’“๐’—๐’Š๐’„๐’† ๐’“๐’๐’ƒ๐’๐’•๐’Š๐’„๐’” ๐’‚๐’‘๐’‘๐’๐’Š๐’„๐’‚๐’•๐’Š๐’๐’". The robotic system was designed by the Italian Institution of Technology of Genoa, in collaboration with SDA Engineering, Ubisive, and the Polytechnic University of Marche, and realized thanks to the synergy with Innse-Berardi, Ingersoll Machine Tools and Camozzi Advanced Manufacturing, companies of the Camozzi Group.

Luca Molinari, Innse-Berardi Chief Operation Officer, and Ferdinando Cannella, IIT Coordinator of Industrial Robotics Facility, have collected the prize at MECSPE.


THE ROBOTIC SYSTEM:

The robotic system is based on the installation of 4 robots on the sides of the bridge: 2 of them will be in charge of inspecting the lower surface of the deck and processing the data in order to find any anomalies (Robot-Inspection) and the other 2 will be cleaning the wind barriers and solar panels (Robot-Wash).

This Robotic Inspection system is the first automatic system in the world and provides a replicable model at the global level designed to enhance the safety of this type of infrastructure and of any civil works that may require automatic monitoring.


"ROBOTIC INNOVATION 2022" AWARD:

The "Robotics Innovation 2022" Award is organized by Automatione Integrata magazine and is dedicated to companies, startups, universities, research centers, laboratory spinoffs, owners of an innovative application as technology providers, system integrators and end users.

In addition to the Main Prize, two special prizes are awarded in the HORIZONS and FOOD sections.

Applications were evaluated by the Technical Scientific Committee (STC) appointed by Automazione Integrata magazine.


 

MECSPE 2022: Camozzi Group and the Italian Institute of Technology have won the "Solution Award"
Related products
MasterPrintยฎ 3X
Masterprint
Ingersoll Machine Tools industry-leading solution for additive manufacturing of complex geometry, durable, XXL, thermoplastic parts.
MasterPrintยฎ 5X
MasterPrint 5X
MasterPrint ® 5X is Ingersoll Machine Tools’ 5 axes version of its MasterPrint ® 3D printer