Camozzi Automation, already associated with A.I.MAN., is a Platinum Sponsor of EuroMaintenance 2024, the premier European event supporting maintenance professionals. The event, which will take place from September 16 to 18 at the Palacongressi in Rimini, is a key moment for discussions with numerous industry experts, but above all, it is a unique opportunity to showcase the main technological innovations for the sector.
MEET OUR EXPERTS AND EXPLORE CUTTING-EDGE TECHNOLOGIES AND PRODUCTS FOR PREDICTIVE MAINTENANCE
If the interconnection of machinery, enabled by the so-called Industrial Internet of Things (IIoT), was the essential element of Industry 4.0, with Industry 5.0 we are moving towards further technological evolution. In addition to the now established need for interconnection, the key concept of predictivity is introduced, based on the ability to collect and organize refined data on the behavior of a component or machine, which can be clearly and legibly presented to an operator, enabling them to monitor and understand its health status at any given moment.
Interconnection and predictivity together lay the technological foundations for the development of so-called Maintenance 5.0 or predictive maintenance, which today becomes a true strategic asset to meet new challenges of energy efficiency, cost, and waste reduction, and to drive the development of increasingly green manufacturing and industry.
It is precisely within this framework that Camozzi Automation supports and participates in Euromaintenance 2024, with a stand dedicated to its range of smart products. Thanks to the ability to integrate pneumatic, proportional, and electric technology, the company offers products and solutions oriented towards predictivity based on a proprietary technology called CoilVision. CoilVision, already integrated into several components including the valve island Series D and the pressure regulators Series PRE and PME, consists of a control algorithm that monitors the health status of the valves inside the mentioned products. This algorithm allows the generation of refined data within the component itself, accessible to the user through LED blinking on the product, or via messages on field buses to the PLC, or through IIoT protocols with WiFi connection to gateways and/or HMIs. Finally, the same data can be accessed through UVIX software, Camozzi Automation's free platform installable on i386 architectures in Linux and Windows environments.

TRY CAMOZZI AUTOMATION DYNAMIC DEMO WITH OUR SMART SOLUTIONS
At the booth, there will be a dynamic demo created in partnershiot with Bi.Lab. It is a perfect example of synergy and integration between the various technologies of Camozzi Automation, as it showcases integrated smart solutions that combine pneumatics, mechanics, and electronics. The cobot in the demo is equipped with the new collaborative gripper, Series CSSP, while the SECO HMI panel allows for data processing and visualization, as well as controlling various machine functions. This demonstrates how refined data can be used and organized through different graphic interfaces designed to maximize the user's experience. Additionally, on this sophisticated demo, you will be able to see the operation of some of Camozzi Automation's most innovative products, such as the valve island Series D, Series DRVI, and the FRL MX Safemax, compliant with the Machinery Directive 2006/42/EC.
DIGITALIZZAZIONE E SOSTENIBILITA’: I MEGA TREND DELLA MANUTENZIONE
EuroMaintenance sarà anche l’occasione per parlare di trend tecnologici e di direzioni evolutive per il comparto della manutenzione, che è ormai un asset strategico per tutte le aziende e che è destinato ad essere uno dei fattori chiave per la transizione digitale e green di tutta l’industria. Camozzi Automation contribuirà a questo dibattito attraverso due contributi dedicati proprio al contributo essenziale che la meccatronica e i prodotti smart possono dare allo sviluppo della manutenzione 5.0:
DIGITALIZATION AND SUSTAINABILITY: THE MEGA TRENDS OF MAINTENANCE
EuroMaintenance will also be an opportunity to discuss technological trends and evolutionary directions for the maintenance sector, which has now become a strategic asset for all companies and is set to be one of the key factors in the digital and green transition of the entire industry. Camozzi Automation will contribute to this debate with two contributions specifically focused on the essential role that mechatronics and smart products can play in the development of Maintenance 5.0.
- Monday 16 September 2024
h 12.15 | Room 6
The Strategic Role of Smart Components and Platforms in the Evolution of the Machine towards an Integrated Communication System
Fabio Bottarelli, Head of Products, Camozzi Automation

- Wednesday 17 September 2024
h 12.15 | Room 6
Mechatronics: the value of the refine data in the component
Andrea Camisani, R&D Director, Camozzi Automation

Read the full program of the Congress area here.