Menu

Camozzi news

 

Camozzi news

Save the date: IMTS 2024 Chicago, USA

18.07.24
Projects
di lettura

Come to visit us!  9-14 September 2024

McCormick Place | South Building Level 3 - Booth 338004

 GET YOUR TICKET

Camozzi Machine Tools, the division of the Camozzi Group that includes Innse-Berardi and Ingersoll Machine Tools, is thrilled to announce its participation at the International Manufacturing Technology Show (IMTS) 2024. The booth is located in the South Building - Level 3 - Nr. 338004.

The International Manufacturing Technology Show 2024 held in Chicago, Illinois from September 9-14. This first-class event showcases the latest advancements in manufacturing technology, robotics, automation, and digital transformation. Offering one of the greatest opportunities to get in contact with the World’s most relevant and well-known innovators, manufacturers, and vendors, and to discover cutting-edge solutions in the industry.


Innse-Berardi & Ingersoll: Your Tech Partners

Camozzi Machine Tools, represented by Ingersoll and Innse-Berardi will showcase their cutting-edge machining solutions designed to meet the demands of the global manufacturing industry. With a focus on precision, efficiency, and sustainability. These technologies are crafted to enhance productivity and drive technological progress.


Subtractive Manufacturing 

Subtractive manufacturing, commonly referred to as CNC machining, is a process based on removing material from a rough piece, or workpiece, to create the desired shape. This can be done through various machining processes such as milling, turning, and drilling. The final piece is obtained after the removal of excess material by means of proper tools designed to reach many kind of geometry. This makes subtractive manufacturing ideal for industries like aerospace, automotive, general mechanic, energy and naval, that require high accuracy and tight tolerances.

Innse-Berardi offers a comprehensive range of products able to reach the best performances in subtractive manufacturing. The Atlas family features vertical multitasking machining centers, while the Aries family comprises advanced horizontal boring and milling machines, both equipped with either hydrostatic or mechanical technology. Additionally, the PowerMax® family specializes in high-speed milling and trimming of large, complex-geometry parts in aluminum, titanium, hard metals.


Additive Manufacturing

Additive manufacturing, usually referred to as 3D printing, is a process based on the realization of objects layer by layer starting from a digital model. This technology works with materials like plastics, metals, and composites, which are deposited and fused to form the final product. AM allows to machine complex geometries and designs that are difficult or impossible to achieve with traditional methods. It is ideal for prototyping, custom manufacturing, and in sectors such as aerospace, naval, automotive medical, which demand high accuracy and flawless finishing. Ingersoll product portfolio includes the latest state-of-art solutions dedicated to this type of manufacturing. Its MasterPrint® family, one of the world's largest thermoplastic 3D printers, is capable of producing extra-large, hollow parts in a single piece especially for the aerospace and marine sectors.


Fiber Placement

Fiber placement is a process that typically involves the use of composite materials, where continuous fibers (like carbon or glass) are precisely placed and bonded to form a composite structure. This method allows for the creation of lightweight and strong components, commonly realized in aerospace, automotive, and sporting goods industries. The fibers are placed using automated machinery that ensures high precision and consistency, optimizing the strength-to-weight ratio of the finished product. Ingersoll positions as a pioneer and significant player in fiber placement manufacturing. Having designed products likeMongoose™, Mongoose Hybrid™, and Hawk™ systems offers to the market advanced and highly capable technologies that are essential for the composite manufacturing of aircraft, rocket, and vessel structures.


Join us at IMTS to discover all our innovative and highly efficient solutions!

GET YOUR TICKET

IMTS2024, Chicago, ILL
Related products
PowerMax® T
PowerMax® T
Innovative large manufacturing center for Titanium and Tough material Applications   
PowerMax® ST
PowerMax® ST
Innovative large manufacturing center for high-performance applications 
Atlas Vision GU
Atlas Vision
The Atlas Vision Gu is an overhead gantry milling center, available from medium to very large sizes.
Additive Manufacturing
Additive Manufacturing
MasterPrint ® , the world largest format gantry and robotic 3D-printers
Aries Vision
Aries Vision
High speed, top performance boring and milling center with linear guideways and roller pads, suitable for 3 and full 5 axes machining.
Atlas Hydro
Atlas Hydro
Range of heavy duty medium and large size vertical milling centers with hydrostatic guideways, suitable for machining large components.
Atlas Vision
Atlas Vision
Family of high speed vertical milling centres, with linear rolling guideways. Innse-Berardi’s innovative flexible design concept is the basis of these ...
Atlas Vision P-W
Atlas Vision
The Atlas Vision P-W machining center is a fixed gantry and moving table. It is a Turning and Milling machine. 
Composite Manufacturing
Composite Manufacturing
Mongoose™, Hawk™ and Mongoose Hybrid™, the most versatile equipment for composite parts manufacturing