Camozzi news

 
 
 
Menu

 

Camozzi news

Camozzi Automation and UniBo Motorsport: A Renewed Partnership for Another Thrilling Year!

21.06.23
Social commitment
di lettura

On June 29 the 2023 Unveiling at Autodromo Nazionale Enzo e Dino Ferrari in Imola

As a technological partner, Camozzi Automation was present at the UniBo Motorsport 2023 Unveiling of the prototypes that will be competing in the races of the current season.

The team, consisting of more than 250 students from various faculties, unveiled the new vehicles that will compete in the Formula SAE and MotoStudent championships:

  • Combustion car Integrale 636
  • Electric car Elettra GN
  • Electric motorbike Minerva GN

During the evening, the UniBoAT (University of Bologna Argonauts Team) training project had the opportunity to present its zero-emission boat. The 1:10 scale driverless prototype was also showcased.


THE TECHNOLOGICAL SPONSORSHIP

Camozzi Automation is glad to be a part of this creative academic initiative with its expertise and solutions:

  • Stainless Steel Fittings INOX 316L: suitable for industrial applications demanding secure solutions that resist high operating temperatures, this range is also highly resistant to corrosion and contamination. Our stainless steel fittings are the ideal solution for the Elettra GN battery cooling system.

  • ISO 6432 Cylinders with Auto-Cushioning Series 23: thanks to a patented system, these cylinders automatically adjust the cushioning to provide optimal deceleration under every condition. During the entire cushioning phase, the cylinder enjoys smooth, jolt-free movement, reducing vibrations and noise while guaranteeing higher reliability and consistent performance over time. These cylinders allow the shift of the gearbox of the Integrale's endothermic engine.

  • Direct-acting Proportional Valves Series AP: manufactured to optimise and reduce friction and stick-slip effects, the output flow is proportional to the control signal. As they can also work in vacuum, minimum working pressure is not required. These valves allow control of the gearbox of the Integrale's endothermic engine.

  • Open Frame Proportional Controller Series OF: closed loop control of flow, pressure, and position designed for Industry 4.0 applications. It can be easily configured to meet specific application needs, to provide the most efficient, turnkey solutions, thus reducing assembly times and system complexity.

CAMOZZI AND MOTORSPORT

Camozzi has a long and successful track record within the world of Formula One, thanks to its expertise in a wide range of sectors.

In 2022 the Camozzi Group returned as an official sponsor of the Alfa Romeo F1 Team through a technological and sporting partnership with Sauber Technologies, the Sauber Group’s entity dedicated to translating the company’s motorsport know-how into the wider world.